המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Automatically launch and login to PME Vista when Windows starts.

Issue

Create a batch file and add it to the Windows startup folder in order to launch Vista and login when Windows starts.

Product Line

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Power Monitoring Expert Vista

Cause

User is requesting an automatic login for Vista

Resolution

1) Create a new text file

2) The first line of code should be browsing to the Power Monitoring Expert\system\bin folder on the computer.

e.g.
cd C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\bin

3) The second line of code should be launching Vista with the username and password specified

e.g.
vista.exe -U<username> -P<password>

4) Now save and then rename the text file to have a .bat file extension instead of .txt
5) Test that the file works by double clicking on the file
6) press Win + R, type shell:startup to open the Windows startup file
7) Copy the .bat file that was created into this folder.


שניידר אלקטריק ישראל

קבצים מצורפים
vistalaunch.bat [87 Bytes]