המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
I have to know what is the function of the LED in the terminal blocks: AB1FUSE435U5XB. This led indicates, voltage presence, or the fuse failure?

Goals and Symptoms

I have to know what is the function of the LED in the terminal blocks: AB1FUSE435U5XB. This led indicates, voltage presence, or the fuse failure?

Causes and Fixes

The LED indicates that the fuse is open (faulty).


Legacy KB System (APS) Data: RESL200113 V1.0, Originally authored by LaBe on 09/28/2009, Last Edited by LaBe on 09/28/2009
Related ranges: AB1, DB6