המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Setting up the 3720 ACM in PME

Issue:

How to setup and connect a 3720 ACM with ethernet option in ION Enterprise/PME

Product Line:

ION Enterprise

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment:

3720 ACM

Resolution:

1) Open Management Console and add a new ethernet device then add all configurations; group, name, device type, and IP Address like normal.
2) On the same ethernet device configuration page right click in the white area (Highlighted in red) and select Advanced Properties.

Image
3) Change the TCP/IP Port to 3720 ACM with MPE|3721 which should be an option in the drop down menu.

Image

4) Click OK to finish