המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to import ION Enterprise OPC data into PowerLogic SCADA

1. Go to Citect Project Eitor -> Communication -> Express Wizard as per below.


2. Click on Next as per below.


3. Select your current I/O server name in 'Use an existing I/O Server' and click on Next.


4. Type the new device name for the ION Enterprise OPC tags (eg. OPC here) and click on Next.


5. Select 'External I/O Device' and click on Next.


6. Choose 'OPC' under 'OPC DA Client' as per below and click on Next.


7. Type ION.OpcDaServer.1 as per below and click on Next.


8. Click on Next.


9. Click on Finish.


10. Go to Citect Explorer choosing your current project -> Tools -> Import Tags...


11. Select your OPC device name ('OPC' here) for 'I/O Device' and select 'OPC' for 'Database type'.
And Click on 'Browse...' as per below.


12. Click on ION.OpcDaServer.1 as per below and click on OK.


14. Click on Import.


15. A progress bar window will be shown as per below.


16. Tag Import Result window will be shown as per below at the end and click on Yes.


17. You can find the ION Enterrpise tags as per below under Citect Project Eitor -> Tags -> Variable Tags.



Original Author: YJ

Public

All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200951 V1.0, Originally authored by KBAdPM on 01/08/2010, Last Edited by KBAdPM on 01/08/2010
Related ranges: PowerLogic SCADA 7.1