המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Testing Demand Period on ION8600 Using PME/Designer

Issue:

The sliding window demand modules in the ION Revenue Test Framework cannot be reset with a push-button. The “Demand Reset” button resets the values but does not reset the period, causing testing delays.

Product:

ION8600 Meter
ION Revenue Test Framework
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment:

  • ION8600 meters configured with the ION Revenue Test Framework
  • Sliding Window Demand modules used for demand testing
  • PME/ION Designer for configuration and testing

Cause:

The sliding window demand modules are synchronized with the meter’s system clock and only reset at fixed intervals (e.g., 00, 15, 30, 45 minutes for a 15-minute period). This design prevents manual reset of the demand period, limiting flexibility during testing.

Resolution:

Workaround: Modify the ION Revenue Test Framework as follows:

1- Add a Pulse Merge module:

    • Connect Pulse In 1 to Test Dmd Rset of the Test Dmd Rset module.
    • Connect Pulse In 2 to CNV1 On Pulse output of the Test Mode Rset module.

2- Add a One-Shot Timer module:

    • Link its Sync input to the Pulse Out of the Pulse Merge module.

3- Connect the Trigger output of the One-Shot Timer to the Sync input of both KW sd del T and KW sd rec T modules.

1
* red box indicates added modules

Permanent Fix:
Download and apply the corrected framework template for the affected meter models:

  • 8600A_V330_FAC-35S_V3.3.0.0.4.fwn
  • 8600A_V330_FAC-35S-PQ_V3.3.0.0.5.fwn
  • 8600A_V330_FAC_V3.3.0.0.4.fwn
  • 8600A_V330_FAC-PQ_V3.3.0.0.5.fwn
  • 8600B_V330_FAC-35S_V3.3.0.0.4.fwn
  • 8600B_V330_FAC_V3.3.0.0.4.fwn
  • 8600C_V330_FAC-35S_V3.3.0.0.4.fwn
  • 8600C_V330_FAC_V3.3.0.0.4.fwn