המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can the 7x50 meter be upgraded in the field to comply with the EN50160 standard?

Issue:
User would like to enable EN50160 capabilities on an ION7x50 meter

Product Line:
ION7650/7550 Meters

Environment:
Power Metering

Resolution:
The meter can be upgraded in the field to comply with the EN50160 standard, uploading the PQ template attached to this article onto the meter. The template can be uploaded to the meter using ION Setup. There is a  potential issue if the template on the meter is customized, the customized portion will need to be ported over to the new template.


שניידר אלקטריק ישראל

קבצים מצורפים
7650_v370_FAC-PQ-61850_V3.6.0.0.0.dcf [984.62 KB]