המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Do the PowerLogic Drivers (PWRMODBUS, MICROLOGIC, PLOGIC, SEPAM) Support Modifying Interpacket Delay in PowerLogic SCADA?

The PowerLogic drivers serialize all requests sent to the same gateway. A new request is only sent when a previous request is replied to by the device, so the device is never asked to process more than one request at a time.

Unlike in the Modnet driver, PowerLogic drivers do not have an option of delaying sending next request after processing the response. Therefore, no "interpacket delay" is possible with these drivers.

However, setting the CacheRefreshTime driver parameter to an appropriately high value and increasing the Timeout parameter can reduce load on a device and may alleviate issues in which modifying the interpacket delay might seem necessary.

Keywords: PLS, PL SCADA, PLSCADA, 7.10, 7.20


Legacy KB System (APS) Data: RESL207045 V1.0, Originally authored by AnVa on 01/04/2012, Last Edited by AnVa on 01/04/2012
Related ranges: PowerLogic SCADA 7.20, PowerLogic SCADA 7.1

AEDL3