המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How to set up SMTP server for Web Applications Reports email subscriptions in ION Enterprise, SPM or PME

Issue
In order to schedule Web Application reports to be sent to an email address, the SMTP server name along with a "From" Email Address will need to be entered into the Reports Configuration Subscriptions via Management Console.

Product Line
Power Monitoring Expert (PME) 7.2.X, 8.X
StruxureWare Power Monitoring (SPM) 7.0.1
ION Enterprise 6.0.1

Environment
SMTP server setup for report subscriptions

Resolution
To configure the SMTP server for email subscriptions in ION Enterprise, SPM or PME, open Management Console and go to Tools-> Reporting Configuration -> Reporting Configuration Manager (NOTE: In PME 8.2, open Management Console and go to Tools -> Reports Configuration). On the Subscriptions tab, you can enter your SMTP server information and "From" email address.

Example subscription settings