איך נוכל לעזור לך היום?

Does the PM8ECC or the CM4ECC (ECC21) support BACnet?

Issue
User wants to know if PM8ECC or the CM4ECC (ECC21) supports BACnet

Product Line
PM8ECC
ECC21

Environment
BACnet communication

Resolution
The PM8ECC and the CM4ECC do not support BACnet. The only protocol supported with the ECC's is Modbus TCP/IP and on the serial side, ModusRTU, JBus, and Symax.