המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is there a Retentive Timer available for Unity Quantum?

Issue:
Retentive timer  for Unity Quantum


Product Line:
Quantum, Unity Pro


Resolution:
No. Using the EN pin will freeze the outputs, but the internal timer keeps running on the TON and TOF blocks. Attached are two user created DFBs that can be used as a Pause/Retentive timer with Unity Quantum.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

שניידר אלקטריק ישראל

קבצים מצורפים
FAQ FA213812 Files.zip [1.72 KB]