המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
B814 Fuse Replacement

Goals and Symptoms

This resolution contains information which enables users to replace the internal 3AG Fast Acting Glass Body fuses that are in series with AS-B814-108 outputs.

Causes and Fixes

B814 fuses can be accessed by removing a plate which covers the option jumpers. In the illustration the plate has a Caution label on it. Four screws need to be removed to free the plate.

AS-B814-108

Fuse part numbers: Schneider 57-0083-000

        • Littelfuse 312007
          Bussman MTH7

Legacy KB System (APS) Data: RESL180177 V1.0, Originally authored by WeDa on 10/23/2006, Last Edited by WeDa on 10/23/2006
Related ranges: Modicon 1/2/3/4/5/8/984s