המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
171CCC9x030 M1E Processor IEC Exec. Upgrade to v.1.30e

Issue
The purpose of this resolution is to inform Momentum M1E users that the IEC Exec. has been upgraded (Aug. 2008) to version 1.30.


Product Line
Momentum


Resolution
IEC Exec version 1.30 resolves the following issues:

1) M1E IEC Exec version 1.29 did not allow OFS to access Concept IEC unlocated variables.

2) An xxmit Function Block in an M1 Processor may fault with an error 150 (in the xxmit block) if the M1 is power cycled a number of times and the xxmit block is active (powered) when the PLC is powered down.

Installing IEC Exec. v.1.30 resolves the above-mentioned issues.


Legacy KB System (APS) Data: RESL192559 V1.0, Originally authored by DaDz on 08/22/2008, Last Edited by DaDz on 08/22/2008
Related ranges: Modicon Momentum