המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
TSXETC101 Explicit Messaging CIP Modbus Object Read Example

Issue
The attached document is a CIP Modbus Object Read example for a TSXETC101 using the Send_Req block to read from a Quantum 140NOC77101.



Product Line
Premium TSXETC101

Quantum 140NOC77101
M340 BMXNOC0401


Resolution
This example will read from located registers in Schneider PLC's with the following network modules installed:

  • TSXETC101
  • 140NOC77101
  • BMXNOC0401

This example does not apply to reading from located registers in Schneider PLC's through the following network module:
  • 140NOC78000



(Removed File URL: 210428_45B6/TSXETC101_CIP_Modbus_Object_READ_Example.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/b0d88c9927345b0dc1257afe002cc849/fl_block_5/0.120?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL210428 V1.0, Originally authored by DaDz on 01/25/2013, Last Edited by DaDz on 01/25/2013
Related ranges: Modicon Premium

שניידר אלקטריק ישראל

קבצים מצורפים
TSXETC101_CIP_Modbus_Object_READ_Example.pdf [128.14 KB]