המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can the scale factor for the Energy readings be changed on the Series 700 Power Meter?

Issue:

Can the scale factor be changed on the PM700 meters

Product Line:

PM700 meters

Resolution

The scale factor for the Energy reading in the Series 700 Power Meter is automatically adjusted by the meter. The front display will adjust based on the range of the reading. There is a scale register associated to Energy but is not user adjustable. Energy is stored in a 2 register format as a floating point value. Other Meters like the Series 2000, 3000, 4000 Circuit Monitors and the Series 800 Power Meter store Energy in 4 registers with a Modulo 10,000 (mod10) format.

For a list of other ION meter rollover values, please see the following https://www.se.com/us/en/faqs/FA239195/