המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Possible Reason for Firmware Failure in 7300

Issue
Firmware upgrade fails in ION Setup and the Device Upgrader, but does not have a specific error code. A general message of "Operation Failed!" or "Upgrade Failed at..."… is given.



Product Line
ION7300

Cause
In this case the firmware version is not compatible with the meter’s Revision. A or B firmware is being installed on a B or A meter. The upgrade fails immediately since the firmware and meter are incompatible.

Resolution
Use the correct firmware version for the revision.
73xx:
Revision A if the last two digits are <= 09
(e.g. PA-0005A123-06)
Revision B if the last two digits are >= 10
(e.g. PA-0005A123-11)