איך נוכל לעזור לך היום?

Series 2000 Circuit Monitor (CM2000) frequency reading is 32,767

Product Line:
CM2000, CM2250 series circuit monitors

Resolution:
It is possible that the frequency reading on a Series 2000 Circuit Monitor (CM2000) will read 32,767 when all other readings are correct. This is typically caused when the nominal frequency setting in the meter does not match that of the actual system being metered. Example: The system being metered is a 400HZ system but the meter nominal frequency setting is still set at the default of 60HZ.