המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where is the 0-10vdc analog input speed reference wired on the ATV71 / ATV61 drives?
Issue:
ATV61/ATV71 speed reference wired installation with 0-10Vdc analog input.

Product Line:
ATV71  ATV61

Environment:
All

Cause:
Wiring 0-10vdc input

Resolution:
Typically, 0-10vdc analog input reference is connected between AI1 (+) and com.

Please note there is a jumper between AI1- and com. Leave this jumper in place. If the jumper were removed, AI1 would become a bipolar (-10 to +10V) input.

Programming:
Menu 1.5, AI1 configuration, choose 0 min and 10vdc max.
AI2 can also be configured for a voltage reference in the I/O menu (1.5).  Under AI2 configuration, select assignment " voltage type" , minimum and maximum values 0 to 10vdc..