המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why do I get an error, "Error 2010: [Switch] [Logout] [When Touch] invalid selection", after adding a Log out object from the Toolchest.

Title
Why do I get the erro: "Error 2010: [Switch] [Logout] [When Touch] invalid selection", after adding a Log out object from the Toolchest.

Issue
To make customers aware, that in order to use any security objects from the toolchest, Target security needs to be enabled.

Product Line
Vijeo Designer

Resolution

You will get this error message if you do not have security setup for the target and have added the Logout object from the Toolchest.  Once you enable target security, that will resolve the error on the build.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)