איך נוכל לעזור לך היום?

What is the Enercept Voltage Lead Length?

Issue:
What is the Enercept Voltage Lead Length?

Product Line:
Enercept Meter

Environment:
Enercept Meter

Resolution:

The voltage lead is approximately 40" from the CT.  From the end of the fuse box to the end of the voltage lead it is about 24"

Voltage Lead Length