המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the part number for the power terminal shrouds for the ATS22C11S6U Soft Starter?

Issue:
Part number request for the power terminal shrouds for the ATS22 series Soft Starters

Product Line:
ATS22 series soft starters.

Environment:
ATS22C11S6,S6U..C17S6,S6U and ATS22C21S6,S6U..C59S6,S6U   All serial numbers.

Cause:
Customer has requested optional terminal shrouds.

Resolution:
For the ATS22C11S6,S6U through ATS22C17S6,S6U, the part number is LA9F702.
For the ATS22C21S6,S6U through ATS22C59S6,S6U, the part number is LA9F703.

The thermal shroud kit includes a set of 6 power terminal protection shrouds.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: