המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What does code SOC mean on the ATV61 and ATV71 drives?

Issue:
What does the condition code SOC mean on the ATV61 and ATV71 drives?

Product Line:
Alivar ATV61 and ATV71

Environment:
All

Cause:
There is a output contactor and the drive is programmed output contactor command is set to OCC

Resolution:
SOC means the OCC output contact cut is active or the motor is disconnected and OPL is set to OCC  with a run command on the drive. .
Try checking the motor connections on UVW or T1 T2 T3 make sure the motor leads are connected.
Try setting OPL to NO and running the drive open circuit to check output voltage on UVW or T1 T2 T3 motor leads.