המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can you find the dimensions for the enclosed 22U soft starters?

Issue:
Enclosed 22U dimensions.

Product Line:
8639/8638 22U, 22T, 22F soft starters

Environment:
Enclosed ATS22

Cause:
Needs dimensions on the 125HP 480VAC with no reversing isolation

Resolution:
You can find the dimension in the enclosed ATS22 22U install manual document 30072-453-26.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)