המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can the voltage boost be adjusted on an ATV312 drive?
Issue:
Needs to adjust the voltage boost, on an ATV312 drive.

Product Line:
ATV312

Environment:
All

Cause:
Need for more voltage on startup.

Resolution:
Go to SEt menu
[IR compensation]  0 to 100%  default is 20%
- For [U/F mot 1 selected] (UFt) = [SVC] (n) or [Energy sav.] (nLd), : IR compensation
- For [U/F mot 1 selected] (UFt) = [Cst. torque] (L) or [Var. torque] (P), : Voltage boost
Used to optimize the torque at very low speed (increase [IR compensation] (UFr) if the torque is insufficient).
Check that the value for [IR compensation] (UFr) is not too high when the motor is in a hot state otherwise some
instabilities can occur.
Note: Changing [U/F mot 1 selected] (UFt), will cause [IR compensation] (UFr) to return to its factory setting (20%).