המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How do I change the Alarm sound in Power Monitoring Expert?
Issue
A user would like to change the Alarm sound in Power Monitoring Expert.

Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

Environment
Power Monitoring Expert Web Applications

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).*

In PME 7.2.x, 8.x, and 9.0 the AlarmSound.mp3 file can be found in:

\\Power Monitoring Expert\Applications\ApplicationFramework\ClientBin\Applications\AlarmViewer\Assets

In PME 2020 the AlarmSound.mp3 file can be found in:

\\Power Monitoring Expert\applications\SystemDataService\Content\Applications\Alarms\Content\Media

Replace this file with a desired .mp3 and rename it to AlarmSound.mp3.