המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is a line reactor required with a ATV312 600V drives?

Issue:
ATV312 600V drive requirement of a line reactor.

Product Line:
ATV312  ATV31

Environment :
All  575-600V

Cause:
New installation

Resolution:
Yes, a minimum 3% line reactor is required on all 575V / 600V drive installations.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)