המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does PM5000 series supports High leg Delta wiring?
Issue
Customer wants to know if the PM5000 series can be wired as high leg delta or not?

Product line
PM5110, PM5330, PM5340, PM5560, PM5563

Environment
Application requires the installation of a power meter or replacement existing meter in a high leg delta system.

Resolution
Yes, PM5000 series can be wired as a high leg delta with the system type as 3-phase 4-wire center-tapped delta.
In addition, the PM5000 series meter can be set to 3-phase 4-wire open center-tapped delta in a case of a three-phase load is small relative to the total load.
In this case, two individual transformers may be used instead of the three for a "full delta" or a three-phase transformer.

The PM5000 series can support all the power system listed below in table. For the wiring diagram, refer to the installation guide for each model of PM5000 series.
Meter SettingPower System Description
1PH2W LN
Single-phase 2-wire line-to-neutral
1PH2W LL
Single-phase 2-wire line-to-line
1PH3W LL with N
Single-phase 3-wire line-to-line with neutral
3PH3W Dlt Ungnd
3-phase 3-wire ungrounded delta
3PH3W Dlt Crnr Gnd
3-phase 3-wire corner grounded delta
3PH3W Wye Ungnd
3-phase 3-wire ungrounded wye
3PH3W Wye Gnd
3-phase 3-wire grounded wye
3PH3W Wye Res Gnd
3-phase 3-wire resistance-grounded wye
3PH4W Opn Dlt Ctr Tp
3-phase 4-wire center-tapped open delta
3PH4W Dlt Ctr Tp
3-phase 4-wire center-tapped delta
3PH4W Wye Ungnd
3-phase 4-wire ungrounded wye
3PH4W Wye Gnd
3-phase 4-wire grounded wye
3PH4W Wye Res Gnd
3-phase 4-wire resistance-grounded wye


See attached document for system type descriptions.

שניידר אלקטריק ישראל

קבצים מצורפים
System.pdf [367.17 KB]