המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What can cause an EPHO on an ATV212 drive?

Article available in these languages: Turkish

Issue:
EPHO on an ATV212 drive

Product Line:
ATV212

Environment:
All models and serial numbers

Cause:
Loss of one or more output phases

Resolution:
Be sure that you're running a 3-phase motor. Altivar drives cannot be used on single phase motors.
Determine the cause of the missing output phase (such as a bad connection, an output disconnect, or an open winding in the motor), and resolve it.
Check parameter F605 (Output Phase Loss). This should be set to 0 (disabled) if you're using a bypass contactor with this drive. It can also be set to 0 for testing purposes.