המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
BMXNOE0110 PV11 Firmware Compatibility Issue
Issue
This Resolution explains a firmware compatibility issue with the BMXNOE0110 at PV11.


Product Line
BMXNOE0110


Resolution
Component obsolescence required a replacement part for the BMXNOE0110's.  Modules with the new flash component are identified as PV11, which resulted in a new firmware version 5.9.
  • BMXNOE0110's at PV11 or higher are only compatible with firmware versions 5.9 or higher.
  • BMXNOE0110's at PV11 or higher cannot be downgraded with firmware versions lower than v5.9.
  • BMXNOE0110 firmware version 5.9 and higher are compatible with all BMXNOE0110 PV versions.