המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can the time duration be defined for a Current Limit status in an ATV61/71?

Article available in these languages: Spanish

Issue:
Torque limitation and current limitation times adjustments

Product Line:
ATV71 ATV61

Environment:
All

Cause:
Need to delay current limit before the drive trips on fault.

Resolution:
Yes, the VFD can be configured for an action when status goes to CLI, current limitation, and after a time delay.
Goto menu 1.8 FAULT MANAGEMENT (FLt)
Goto submenu TORQUE OR I LIM. DETECT (tid-)
Select parameter Trq/I limit. stop (SSb) and set to the desired behavior in the event of switching to torque or current limitation.
Select parameter Trq/I limit. time out (Sto) and set the time delay for taking SSF "Limitation" fault into account.