המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do you get the Computer (either Magelis iPC or 3rd party) to boot up and have the Vijeo Designer PC Runtime come up in a minimized state and not full screen?
Issue:
How do you get the Computer (either Magelis iPC or 3rd party) to boot up and have the Vijeo Designer PC Runtime come up in a minimized state and not full screen?
Product Line:
Vijeo Designer PC Runtime, iPC, Magelis Box PC, Magelis Panel PC
Resolution:
To get Vijeo Designer PC Runtime to run as minimized on boot up.  You need to do the following:

Launch Vijeo Designer Runtime Manager and select Disable Autorun.
<Right click> on the Vijeo Designer short cut and select "properties" then select the "short cut" tab. In the run pull down, select "minimized" instead of normal window.
Copy the PC runtime icon to the start up folder.  This will start the the runtime in minimize mode.