המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does Vijeo Designer Web Gate support connections through a Proxy Server?
Issue:
Does Vijeo Designer Web Gate support connections through a Proxy Server?

Product Line:
Vijeo Designer

Resolution:
No, Vijeo Designer's Web Gate feature for HMIs does not support a connection through a Proxy Server.  To use Web Gate you need to configure Port Forwarding on the Proxy Server with the target IP address.  See Section 23.2 of the Vijeo Designer Help.