המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to get the Magelis/Harmony HMI to read a KollMorgen AKD Servo Drive low 32bit word that is 64bit word in the drive?

Issue:
How to get the Magelis/Harmony HMI to read a KollMorgen AKD Servo Drive low 32bit word that is 64bit word in the drive?

Product Line:
XBTG/GH/GK/GT, Smart iPC, Compact iPC, HMIGTO/GTU/STO/STU

Environment:
Modbus Addressing

Resolution:
To resolve the issue you need to go into the Workbench Software(the AKD configuration software) change the drive parameters scale from “MODBUS Scaling"
to “Drive internal”.  (See screenshot below).  The value will come into the Magelis as a double integer, you will need to divide by 1000 to get the correct value.

screenshot

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)