המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where is the biometric switch information stored when using it with Vijeo Designer?
Issue
Where is the biometric switch information stored when using it with Vijeo Designer?

Product Line
Vijeo Designer
Harmony XBS5 Biometric Switch

Resolution
The encrypted fingerprint database is stored in Runtime and in the switch itself. When you configure fingerprints in your VJD application then download to the HMI, the fingerprint database is downloaded along with the project. At Runtime (on the HMI), when you connect the Biometric switch, the Runtime engine automatically downloads the fingerprint database to the device. When you add fingerprints in Runtime, the fingerprint data is stored in both Runtime and in the switch.