איך נוכל לעזור לך היום?

What is the interval for the WebReach/Diagram RMS calculation

Issue
RMS calculation frequency in the Waveform display in WebReach/Diagrams is unknown and no documents explain how often the value is calculated

Product Line
ION Enterprise 6.0
Struxureware Power Monitoring 7.0.x

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024


Environment
Web Applications Diagrams or Web Reach

Cause
Documents do not describe how often RMS is calculated

Resolution
The interval for the RMS calculation is 1 cycle.