המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to resolve error message: "One or more issues occurred with the current version profile. Please contact the vendor to resolve these problems." in Somachine v3.1?
Issue:
How to resolve error message: "One or more issues occurred with the current version profile.  Please contact the vendor to resolve these problems." in Somachine v3.1?

Product Line:
SoMachine

Environment:
PLC Programming Software in Windows

Resolution:
This is an known issue with the installation of SP of Somachine V3.1, when SoMachine was not installed on the default location: "C.\Program Files (x86)\Schneider Electric\SoMachine"

To solve this issue you can move or copy the content of the folder:
"C:\<your installed path>\SoMachine\SoMachine\CoDeSys\PlugIns"
to the correct location
"C:\<your installed path>\Schneider Electric\SoMachine\CoDeSys\PlugIns"

Alternative you can extract and copy the content of the attached zip archive to folder:  "C:\<your installed path>\Schneider Electric\SoMachine\CoDeSys\PlugIns"

Afterward you have to delete the CoDeSys cache file(s) "CoDeSys*.cache" at the following locations: "C:\ProgramData\AP\PlugInCaches\"

שניידר אלקטריק ישראל

קבצים מצורפים
UpdatedPlugins.zip [349.18 KB]
גלה עוד
מוצר:
גלה עוד
מוצר: