המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do you size a full voltage bypass contactor for the open type ATS48 soft starters?
Issue:
Need to size a full voltage bypass contactor for the open type ATS48 soft starters.

Product Line:
Altistart ATS48

Environment:
All

Cause:
Needs to add a full voltage bypass contactor to an open type ATS48 soft starter.

Resolution:
You will size the full voltage bypass contact to the size of the motor amps.   Please note that if you field install a bypass contactor you may need to add a line isolation contactor and add NC contacts so that you can turn off the soft starters control CL1 CL2 control voltage when you are in full voltage bypass.