המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How are date and time shown in Power Monitoring Expert (PME) trends?
Issue
In the trending graphs, sometimes the time is displayed with no date and sometimes it is displayed with both the date and the time.

Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Web Applications "Trending"

Cause
Customers might want to see the date and time in the trending graphs, or just the time.

Resolution
Date and time are shown for trending when 6 hours or longer is selected. For 3 hours or less, only the time is displayed with no date.

Example: Three Hours Trend
Three Hour Trend Example