המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I find out more information about the Powerlogic Branch Circuit Monitoring?

Issue
General information and guides for the Powerlogic Branch Circuit Power Meter (BCPM) product line are required.

Product Line
Powerlogic BCPM, BCPME

Environment
BCPM Documentation

Resolution
The Branch Circuit Monitoring System consists of a main board and up to 84 branch circuit CTs. The CTs can either be solid-core CTs assembled onto a long PCB Board or individual split-core CTs. For more information about product selection, installation, and function, feel free to explore the attached documents.

Included information:
- Brochure
- Technical Data Sheet
- BCPM Installation Guide
- BCPMSC Installation Guide for Split Core CTs
- BCPME User Guide (Ethernet Communication Model)

Link to Full Document Library (includes several other installation guides)
Link to BCPM register list: FA212184

שניידר אלקטריק ישראל

קבצים מצורפים
BCPM_Brochure_3000BR0805R0714V3.pdf [9.18 MB]
Technical_Datasheet_PLSED308011EN.pdf [6.86 MB]
BCPM_Installation_Guide_Z205396-0H.pdf [3.09 MB]
BCPME_User_Guide.pdf [6.82 MB]
BCPMSC_SplitCore_Z205658-0F.pdf [4.2 MB]