המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How many Remote IO drops does an M580 PLC support?

Article available in these languages: Spanish

M580 CPU                      |        Max Remote I/O Drops
--------------------------------------------------------------------------------

BME P58 2040                |              8
BME P58 3040                |              16
BME P(H)58 4040           |              16
BME P(H)58 5040           |              31
BME P(H)58 6040           |              31
--------------------------------------------------------------------------------
A "Rack" is defined as a backplane which holds devices.
A "Drop" is defined as the rack which are connected to CPU as a node on the RIO network.
A Drop can contain multiple racks by use of the BMXXBE Rack Extenders.