המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What can cause the fault code of CF1 when loading a configuration to a drive, using SoMove?
Issue:
CF1 on the display when loading a configuration to a drive, using Somove.

Product Line:
SoMove

Environment:
All versions

Cause:
Corrupt installation of SoMove.

Resolution:
Re-download and install SoMove.  It is recommended using a download manager such as the one from the website www.freedownloadmanager.org .  Download this and have it running in the background prior to downloading SoMove.  You will also need to update your DTM files.