המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can we upgrade PME 7.2.2 running on SQL Server 2008 Express to SQL Server 2012 Standard?
Issue:
Customer is currently running PME 7.2.2 on SQL Server 2008 Express and would like to upgrade it to SQL Server 2012 Standard

Product Line:
Power Monitoring Expert 7.2.2

Environment:
Power Monitoring Expert Software Upgrade

Cause:
Some customers might have installed PME on SQL Express but due to system expansion would like to move to a Standard Edition to avoid database size limitations that come with Express.

Resolution:
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

Attached document goes over steps to upgrade the SQL Edition PME is running on from SQL Express to SQL Standard.

Note: Recommend stopping the ION and Application Module services before performing the upgrade. The Installer will stop the SQL service and all services Dependant on SQL.

שניידר אלקטריק ישראל

קבצים מצורפים
SQL_2008_Express_to_SQL_2012_std_upgrade.pdf [269.2 KB]