המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I find information on the Altivar ATV12, ATV212, ATV312, ATV61 and ATV71 Demo kits?
Issue:
Information request on the ATVFLEXDEMO kit and parts

Product line:
Altivar

Environment:
n/a

Cause:
n/a

Resolution:
See the attached brochure on the DEMO kit and replacement drives that will fit in.

ATVFLEXDEMO01 is obsolete - Set including the ATVFLEXDEM02 and ATVFLEXDEMO03.
ATVFLEXDEMO02 is obsolete and replaced by the DemoATVSIM- control panel and Demonstration box with buttons, pilot lights, simulation inputs/outputs, HMI keypad and miscellaneous controls.  Prewired with pigtail connectors to plug in one of six drives.
ATVFLEXDEMO03 is obsolete - storage ad shipping case with full set of six Altivar drives.  For use with the Demonstration box ATVFLEXDEMO02.  Simple loader and Multiloader included.

Single replacement drives (comes with backplate mounting, and prewired pigtail connectors)
ATV12FLEXDEMO is now obsolete
ATV212FLEXDEMO is now obsolete
ATV312FLEXDEMO is now obsolete
ATV32FLEXDEMO is now obsolete
ATV61FLEXDEMO is now obsolete
ATV71FLEXDEMO is now obsolete

The new ATV Process Drives Demo kits are now called Eco Struxure Demos (click).

שניידר אלקטריק ישראל

קבצים מצורפים
ATV Flex Demo.pdf [185.18 KB]