המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is there a remote extension cable for the Magelis HMISTU655 or HMISTU855?
Cable part numberLengthCompatible
HMIZSURDP3mHMISTU PV07 SV5.0 or greater. Vijeo Designer V6.2 SP2
HMIZSURDP55mHMISTU PV07 SV5.0 or greater. Vijeo Designer V6.2 SP2
HMIZSURDP1010mHMISTU PV07 SV5.0 or greater. Vijeo Designer V6.2 SP2
.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)