המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I find the SCCR ratings for ATV61 or ATV71, 18 pulse enclosed drives ?

Issue:
Looking for the SCCR ratings for ATV61 or ATV71, 18 pulse drives ?

Product Line:
ATV61 / ATV71

Environment:

PowerGard 18 Pulse Drives

Cause:
None

Resolution:
PowerGard enclosed drive controllers have a short-circuti current rating of 100 kA @ 480 V (RMS symmetrical).

See Altivar® 61/71 PowerGard™ Class 8839 Type CPD 18-Pulse Adjustable Speed Drive Controllers Instruction Bulletin 30072-451-53 for details.

https://www.se.com/us/en/download/document/30072-451-53/

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)