המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What can cause an Error 5 on ATV212 or S-Flex?
Issue:
ATV212 or S-Flex showing Error 5.

Product Line:
ATV212, S-Flex

Environment:
All

Cause:
If F829 is not 1 and CNOD is 2, FNOD is 4

Resolution:
To clear the Err5 set F829 to 1, CNOD to 0, and FNOD to 1. This will allow the drive to run from the terminals and use VIA for speed control. This will allow you to test the unit. When communication is set up and if  you are using the communication card for monitoring then set F829 to the correct communication card. If you are using the communication for control then set F829 to correct communication and CNOD to 2 and FNOD to 4.