המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Error: "Request ExecuteCipher fail at function call;ConfigureCipher" during Powerlogic Scada installation
Issue
Customer gets an error during the installation that reads Request ExecuteCipher fail at function call;ConfigureCipher"



Product Line
Powerlogic Scada 7.40

Cause
Powerlogic Scada was installed in the machine preciously and the uninstall did not get rid of all the registry files. This could be either the same version, or an older version.

Resolution
Download the attachment and run the .bat file on server where Powerlogic Scada needs to be installed. Try to install the software again after running the .bat File

שניידר אלקטריק ישראל

קבצים מצורפים
UninstallPSE_7.40.bat [1.79 KB]