איך נוכל לעזור לך היום?

Does the M340 BMXPRA0100 Remote I/O module come with an SD card on delivery?

Yes. The standard SD card part# BMXRMS008MP is included when purchasing the unit BMXPRA0100 Remote I/O module.