איך נוכל לעזור לך היום?

How to manage the interaction between two curves, IDMT and DT, while tripping time of IDMT curve is much faster than DT? This may happen actually at the end of tripping curve.

In this FAQ we give some recommendation to manage the issue of interaction between two curves, IDMT and DT, while tripping time of IDMT curve is much faster than DT. We are going to add some logic equations and another DT setting to fix this issue. Please check the attached file.
AEDL3

שניידר אלקטריק ישראל

קבצים מצורפים
FA243151.pdf [616.19 KB]