המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why is the web page not accessible on ATV61/71 drives?

Issue:
Accessing webpage on ATV61 ATV71 VFDs.

Product Line:
Altivar 61 and 71 drives

Environment:
All models and serial numbers with Ethernet IP option card VW3A3316

Cause:
Java 1.8 is not supported or web server services are not activated.

Resolution:
First, verify that web server services are  activated via the "SERVICES" parameter:
From the main menu, navigate to the DRIVE menu -> [COMMUNICATION] -> [ETHIP] -> [SERVICES] and verify that Web server services are not deactivated.

Next, check your computer's Java version, and if 1.8 or later is installed, roll back the Java version to 1.7.67.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)