המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I find information on dynamic braking resistors to use with the ATV32, ATV312 and ATV71 drives only?
Issue:
Dynamic braking resistors to use with the Altivar drives.

Product Line:
ATV32, ATV312 and ATV71 Drives

Environment:
All

Cause:
Needs to know if the drives come with a DB resistor?

Resolution:
The braking resistor is not included on the ATV32, ATV312 and ATV71 Drives, and if needed must be purchased separately.
In the US, we have partnered with a resistor company named Powerohm to provide a full range of options.
See attached document for information on sizing and selecting DB resistors from Powerohm.
Note that any technical questions related to the resistors themselves should be directed to Powerohm and the document includes their contact information.

שניידר אלקטריק ישראל

קבצים מצורפים
POWEROHM_SELECTION AND PRICE GUIDE_Y13M03D15.xlsx [1.38 MB]
גלה עוד
מוצר:
גלה עוד
מוצר: